2025-08-03 3:39 AM
Hi ,
I am trying to measure the output return loss ( in tx mode) of my board rf chain which include the stm32wle5.
if i understnad correctly - in order to do that i need to put the STM32WLE5 in TX MODE which means its PA should be powered up and ready to transmit but without any transmitted data. ( so that i will be able to measure the Return loss using external VNA connected to the TX RF PORT of my board)
is there an option to do that ? i cant seem to find a way to make the internal PA ready to transmit (powered up) without actually transmitting . is it possible to measure the output RL as i described ?
thank you,
viola
2025-09-19 7:53 AM
Hello @viola
May i know why are you interested in this? Are you experiencing unsatisfactory TX performance that is far from what is stated in the datasheet?
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.