2025-10-17 8:24 AM
Hi,
I was testing the End Node example on a custom board equipped with a STM32WL5MOC module. However, I changed only the UART from UART2 to UART1 in platform settings. I also activate the DMA. However, I can get only "APPLICATION_VERSION: V1.3.1" on the UART terminal and no other messages. Someone knows why?
Thanks.
Matteo
Solved! Go to Solution.
2025-10-17 8:43 AM - edited 2025-10-17 9:08 AM
Solution find. It is necessary to enable the interrupt line of the UART. Hint: change also Preemption priority of the USART interrupt and DMA to 2 otherwise the hw timer won't work anymore,
2025-10-17 8:43 AM - edited 2025-10-17 9:08 AM
Solution find. It is necessary to enable the interrupt line of the UART. Hint: change also Preemption priority of the USART interrupt and DMA to 2 otherwise the hw timer won't work anymore,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.