STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! Main stack pointer stm32wle5xx

Hii try to figure out, if my main stack pointer is correct. When debug my program, after execute startup.s file the value of msp is 0x20008000, but like this i used only half sram, right? This micro have 64KB of sram. I believe that the value of msp ...

en by Associate II
  • 4644 Views
  • 6 replies
  • 0 kudos

Sigfox - trouble at t'mill

In the news today:"Sigfox, the French IoT startup that had raised more than $300M, files for bankruptcy protection as it seeks a buyer"https://techcrunch.com/2022/01/27/sigfox-the-french-iot-startup-that-had-raised-more-than-300m-files-for-bankruptcy...

On STM32 cube I-CUBE-LRWAN, GPIOS sx1276

#define RADIO_TCXO_VCC_CLK_ENABLE()   __HAL_RCC_GPIOA_CLK_ENABLE()#define RADIO_ANT_SWITCH_CLK_ENABLE_RX()   __HAL_RCC_GPIOA_CLK_ENABLE()#define RADIO_ANT_SWITCH_CLK_ENABLE_TX_BOOST()   __HAL_RCC_GPIOC_CLK_ENABLE()#define RADIO_ANT_SWITCH_CLK_ENABLE_...

MWisi.1 by Associate II
  • 3644 Views
  • 7 replies
  • 0 kudos

Resolved! Strange delay on QSPI using 4 data lines

Hi all,Currently i'm reading and writing to external flash using the QSPI peripheral. All data i write is received correctly but there seems to be a "unnecessary" delay in both writing and reading QSPI.Sequence start with command 0x34 (page program)F...

0693W00000JNP7xQAH.jpg
Taxara by Associate III
  • 2922 Views
  • 3 replies
  • 0 kudos

Resolved! Error in AN5566

In the AN5566 RF certification process for NUCLEO-WL55JC, chapter 1.3 talk about ETSI 300-200: Short Range Devices (SRD) operating in the frequency range 25 MHz to 1000 MHz.But there is no ETSI 300-200, the correct is ETSI EN 300 220.

nicolas by Senior II
  • 2003 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.