2026-03-02 6:46 PM
Starting my design on a reference design based on STDES for WL3 series. I would like to know what is needed for the smallest hardware connection to download a program from ST32CUBE IDE. I need to have the minimum amount of connectors on the board. I.E. I don't want to plug in my board that I designed to the NUCLEO base board debugger for downloading a program if I don't have to. Can I take advantage of the STDC14 connection on the ref Des and if so, do I need some external piece of hardware to connect to it which then connects to the USB port on a computer? Thanks!
Solved! Go to Solution.
2026-03-04 6:02 PM
A few things:
Typically it's better to use a standard header like the STDC14 connector and place that on your board instead.
2026-03-04 5:40 PM
Can anyone reply to this question?
2026-03-04 6:02 PM
A few things:
Typically it's better to use a standard header like the STDC14 connector and place that on your board instead.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.