cancel
Showing results for 
Search instead for 
Did you mean: 

stm32wl33c8 Transition Energy

guest1
Associate

Hi there,
for a project at university we need to estimate the power consumption of stm32wl33c8 mcu. One open question is the power needed for transition from deepsleep to waking state as we need to wake the cpu very often over a long time to read out an i2c sensor, read out an analog value with adc and put back to sleep.
So first guess is that most time is needed to stabilize HSI actually, but actually can't find values for it on datasheet. The sensor becomes ready within 5ms.
Hope we'll get good suggestions here.
Best regards

1 REPLY 1
STTwo-32
ST Employee

Hello @guest1 

The best way to know that is to test it in all available conditions. You may thank about using the NUCLEO-WL33CC together with the sensor for evaluation.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.