2025-10-13 1:28 PM
Hello,
I am looking for guidance on how to share the CRC peripheral between two modules. For instance, in our application we are using the BLE stack (for example, following this: https://wiki.st.com/stm32mcu/wiki/Connectivity:STM32WBA_BLE_STM32CubeMX#STM32CubeMX_initial_setup). We also are using the SAI interface to sample PDM microphones, and using the PDM2PCM middleware. The PDM2PCM library has something of a hidden dependency on the CRC being enabled.
My question is - will the two modules conflict? I notice that in app_entry.c there is a mutex being used to control access to the CRC interface (presumably).
How should I ensure that the two requirements don't clash with each other?
Thank you,
Jonathan
Solved! Go to Solution.
2025-10-14 2:37 AM
Hello,
The PDM2PCM library uses the CRC during PDM_Filter_Init() only and bypasses the crc_ctrl.c. At this time the PDM2PCM requires the CRC to be configured with default values (CRC_CR = 0x000000000 and CRC_POL = 0x04C11DB7).
The STM32WBA BLE Framework uses the CRC with a configuration different from the default (for the NVM).
A possibility would be to add a config in the crc_ctrl_conf.c :
CRCCTRL_Handle_t PDM2PCM_Handle =
{
.Uid = 0x00,
.PreviousComputedValue = 0x00,
.State = HANDLE_NOT_REG,
.Configuration =
{
.DefaultPolynomialUse = DEFAULT_POLYNOMIAL_ENABLE,
.DefaultInitValueUse = DEFAULT_INIT_VALUE_ENABLE,
},
};Then register the handle with CRCCTRL_RegisterHandle(&PDM2PCM_Handle); and call CRCCTRL_Calculate(&PDM2PCM_Handle, ...) just before PDM_Filter_Init() with some void parameters to force the CRC reconfiguration. (You must ensure the CRC is not used between these two calls....)
Otherwise, you can do yourself the CRC reconfiguration / restoration around PDM_Filter_Init(). In that case, note the CRC_CR RESET does not reset all registers such CRC_POL.
Best regards,
2025-10-14 2:37 AM
Hello,
The PDM2PCM library uses the CRC during PDM_Filter_Init() only and bypasses the crc_ctrl.c. At this time the PDM2PCM requires the CRC to be configured with default values (CRC_CR = 0x000000000 and CRC_POL = 0x04C11DB7).
The STM32WBA BLE Framework uses the CRC with a configuration different from the default (for the NVM).
A possibility would be to add a config in the crc_ctrl_conf.c :
CRCCTRL_Handle_t PDM2PCM_Handle =
{
.Uid = 0x00,
.PreviousComputedValue = 0x00,
.State = HANDLE_NOT_REG,
.Configuration =
{
.DefaultPolynomialUse = DEFAULT_POLYNOMIAL_ENABLE,
.DefaultInitValueUse = DEFAULT_INIT_VALUE_ENABLE,
},
};Then register the handle with CRCCTRL_RegisterHandle(&PDM2PCM_Handle); and call CRCCTRL_Calculate(&PDM2PCM_Handle, ...) just before PDM_Filter_Init() with some void parameters to force the CRC reconfiguration. (You must ensure the CRC is not used between these two calls....)
Otherwise, you can do yourself the CRC reconfiguration / restoration around PDM_Filter_Init(). In that case, note the CRC_CR RESET does not reset all registers such CRC_POL.
Best regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.