2023-01-03 3:12 AM - last edited on 2023-11-30 6:46 AM by Amel NASRI
after looking over all the documentation i could find (datasheet, reference manual, etc.), i could not clearly find how i am meant to connect IR LED(s) for IrDA communication with an STM32WB55. The image i attached is a screenshot from the reference manual, which implies that there may be IrDA_OUT and _IN pins (i'm interpreting this as being seperate from the TX and RX pins). Am i supposed to add some kind of intermediate IC for IrDA, or can the STM32WB55 actually output signals for driving/reading IR LEDs/photodiodes?
P.S. i'm aware of the existance of the IR_OUT pins, but that appears to be its own seperate thing. In the IR_OUT documentation they use only timers (TIM16 & TIM17), not the USART peripheral.
Solved! Go to Solution.
2023-01-03 5:46 AM
IrDA has hardly been used for a long time, which is also noticeable in discontinued IrDA transceivers. However, since essentially everything except the TIA and optical components is included in the STM32 IrDA SIR ENDEC, it is possible to recreate IrDA with
As @MM..1 said, RX and TX are switched to the IrDA function so that LED driver and TIA can be connected directly.
Regards
/Peter
2023-01-03 4:33 AM
Yes not clean , but i mean TX and RX is changed into IR after HAL IRDA init ...
2023-01-03 5:46 AM
IrDA has hardly been used for a long time, which is also noticeable in discontinued IrDA transceivers. However, since essentially everything except the TIA and optical components is included in the STM32 IrDA SIR ENDEC, it is possible to recreate IrDA with
As @MM..1 said, RX and TX are switched to the IrDA function so that LED driver and TIA can be connected directly.
Regards
/Peter
2023-01-09 3:23 AM
alright, thank you!
2025-03-13 4:51 PM
Thanks for the answer but please explain to me...
Does the carrier frequency modulation happen inside the STM32?
For example, I want to receive data using the TSOP1238 chip. It is based on 38 kHz carrier frequency. Should I connect it directly to the Rx pin of the receiving STM32?
At the same time, the IrDA transmitter (STM32 too) can modulate the data by carrier frequency 38 kHz and I only need a MOSFET and an LED connected to the Tx pin of the transmitter STM32 chip?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.