2022-07-14 2:50 AM
I designed a custom board with STM32WB55 with a USB connection to update the BLE stack in DFU mode.
When I connected the board to my laptop's USB port, it appeared in the device manager and was detected as a USB device, however since yesterday when I was trying to update the BLE stack on STM32WB55, all of the sudden, my laptop can't detect the board anymore.
I can program the board with the ST-link programmer and MCU is functioning, but I can't use DFU mode.
What would be the problem? Why the MCU is not detected by the laptop?
Would it be possible that I remove DUF bootloader by mistake?
2022-07-20 3:13 AM
Hello,
In order to connect your board using DFU mode, the option byte nSWBOOT0 should be checked and BOOT0 pin should be HIGH.
Best Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.