2021-11-03 1:09 AM
A tricky one here,
Migrated the BLE_HearRateFreeRTOS to a keil FuSa project. Using uvision.
During the Init process, the first BLE event that I receive after programming is an " unknown sys evt" .
Trace :
11/03 09:58:21.646 #1 unknown sys evt received: d8
11/03 09:58:21.646 Raw bytes size : 3, data: c8 d8 00
After I press the reset button, and run the program again everything works fine.
Using the STM32WB55.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.