2025-02-20 5:43 PM - edited 2025-02-20 5:44 PM
Hellow all,
I am running a custom BLE application on STM32WB55 and I want to run in low power STOP2 mode,At the same time, Bluetooth needs to remain in broadcasting state. I am not sure what the average power consumption is in this case. I monitored that after CPU1 enters STOP2 mode, the average power consumption is about 6mA. Is this normal? Is there a theoretical minimum average power consumption value that can be achieved when CPU1 enters STOP2 mode and Bluetooth is still broadcasting for reference? Thank you very much!
2025-02-26 8:16 AM
Hello,
you can find theoretical power consumption values in the datasheet. 6 mA is quite high average power consumption, but without more details about your application is not possible to evaluate as average power consumption depends on multiple details
Have you/could you try the measurement also with Beacon example from our repository?
Best regards,
Lubos
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.