2023-03-20 8:52 AM
I am trying to use as little power as possible, I want my board to wake up every 30 seconds or so, check if battery has been sufficiently charged, if not, go back to sleep, if it has then turn off rtc and do a function. Is it possible to disable rtc whilst running?
2023-03-21 7:15 PM
Dear Liam
Our team is checking into this inquiry and we will be in touch with you shortly.
Kind Regards
Joe WILLIAMS
STMicro Support
2023-03-22 11:14 AM
> Is it possible to disable rtc whilst running?
What makes you think the RTCEN bit in RCC_BDCR register cannot be cleared?
2023-03-31 7:26 AM
Hello,
You can disable the RTC by setting the RTCSEL in RCC_BDCR register at no clock.
Best Regards
2023-04-01 2:34 AM
Bits 9:8 RTCSEL[1:0]: RTC clock source selection
Set by software to select the clock source for the RTC. Once the RTC clock source has been selected, it cannot be changed anymore unless the Backup domain is reset, or unless a failure is detected on LSE (LSECSSD is set). The BDRST bit can be used to reset them.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.