2020-01-16 10:58 PM
I am attempting to send Multicast Non-Confirmable coap messages to multiple boards, but am only receiving and handling the first response that comes in.
This seems to be supported in the upstream implementation found at https://github.com/openthread/openthread/blob/master/src/core/coap/coap.cpp#L513.
Can you please confirm whether your OpenThread implementation allows receiving multiple responses or if there is a problem with my implementation.
2020-01-17 7:41 AM
On this point our current OpenThread version is not aligned with the upstream version you are referring to.
So receiving multiple responses when sending Multicast Non-Confirmable CoAP request is not supported.
Our implementation:
case OT_COAP_TYPE_NON_CONFIRMABLE:
// Separate response.
FinalizeCoapTransaction(*message, coapMetadata, &aResponseHeader, &aMessage, &aMessageInfo, OT_ERROR_NONE);
break;
Upstream implementation you are referring to:
case OT_COAP_TYPE_NON_CONFIRMABLE:
509 // Separate response.
510
511 if (coapMetadata.mDestinationAddress.IsMulticast() && coapMetadata.mResponseHandler != NULL)
512 {
513 // If multicast non-confirmable request, allow multiple responses
514 coapMetadata.mResponseHandler(coapMetadata.mResponseContext, &aMessage, &aMessageInfo, OT_ERROR_NONE);
515 }
516 else
517 {
518 FinalizeCoapTransaction(*request, coapMetadata, &aMessage, &aMessageInfo, OT_ERROR_NONE);
519 }
520
521 break;
2020-01-19 8:37 PM
I see that your implementation is based on github here:
https://github.com/openthread/openthread/commit/222acd1362af9f5b58bae9d246fe5492c38e7b14
dated 13/9/2018.
The fix is implemented upstream on github here:
https://github.com/openthread/openthread/commit/6a2c3ba10cc66c2939c1b86a78e56ebec882bc4b
dated 10/7/2019.
Do you have any plans to rebase onto a more up to date upstream implementation or to to open source your implementation?
2020-01-20 1:31 AM
I will push the fix to the development team but I cannot commit about any new rebased version for the short term as I know they have a lot of higher priority developments to complete before.
2020-01-21 2:14 PM
There are a large number of fixes to this codebase since ST grabbed the source from Github, with some pretty major fixes included.
I would have understood that a rebase would have been critical path for ST considering it would have reasonable affect to anyone trying to use Thread on a STM32WB
This is even more critical since users cannot update the code themselves as the ST implementation is closed source.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.