2021-07-21 11:34 PM
Slave can configure his MAC address either in the payload or internally. This I know.
My question is , after connection, does the masters packets hold that (slaves) MAC address?
Can Slave extract (its own) MAC address from the Masters packets?
If, so , how can slave get hold of this data from code?
2021-08-19 5:47 AM
Thanks, does CPU2 has an event for CPU1 in case of a CONNECT_REQ packet?
I am using the BleHeartRateFreeRTOS example.
If not, how can I get hold of that packet?
2021-08-19 9:11 AM
Yes! this is the HCI_LE_CONNECTION_COMPLETE_EVENT event that is processed via the hci_le_connection_complete_event (...) function.
The LE Connection Complete event indicates to both of the Hosts forming the
* connection that a new connection has been created. Upon the creation of the
* connection a Connection_Handle shall be assigned by the Controller, and
* passed to the Host in this event. If the connection establishment fails this
* event shall be provided to the Host that had issued the LE_Create_Connection
* command.
* This event indicates to the Host which issued a LE_Create_Connection command
* and received a Command Status event if the connection establishment failed
* or was successful.
2021-10-07 5:31 AM
Hi, almost there,
On HCI_LE_CONNECTION_COMPLETE_EVENT I get this payload:
Payload 20002d7c:
01 FF FF FF F4 02 03 20 F4 02 03 20 90 2D 00 20 3F F0 00 08 A5 A5 A5 A5 00 00 00 00 A5 A5 A5 A5 49 DC 00 08 A5 A5 A5 A5 A5 A5 A5 A5 00 00 00 00 68 00 00 80 E4 2C 00 20 00 00 00 00 94 1B 00 20 94 1B 00 20 B0 2D 00 20 8C 1B 00 20 20 00 00 00 00 00 00 00 00 00 00 00 B0 2D 00 20 00 00 00 00 18 00 00 00
Then the PDU is at 0x200302F4:
74 01 00 20 74 01 00 20 04 3E 13 01 00 01 08 01 00 2A 6A CF 50 A0 00 07 00 00 00 0A 00 07 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
2A 6A CF 50 A0 00 is the the clients address.
According to picture it should be the 6 previous bytes, but that is not my (=server) address.
Where can I see my address?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.