2020-09-11 7:24 AM
Hi All,
I have recently purchased the ST-LRWAN2 package.
I have successfully setup the LoRaWAN Gateway.
But I am not able to setup the Node device NUCLEO-L073RZ.
I am using STMCubeIDE. The software package I am using is i-cube-lrwan.
I am not able to see any output on the Serial monitor
I have attached the images for more details.
If anyone has successfully setup the device, please advice on this.
Thanks and Regards,
Rahul
2020-10-06 12:02 PM
Hello,
i use a B-L072Z-LRWAN1-board, so i make a new projekt (I-Cube) and select this board, i generate the code.
How can i use the files from I-CUBE-LRWAN firmware package (STM32CubeExpansion_LRWAN_V1.3.1). For Lorawan-example there is an Irc and Src-folder with separate main.c?
Then you must configure your node First are you using ABT or OTTA?
Wich Region you select (868Mhz for Europe)?
Greetings
E_T
2021-01-23 10:53 AM
A bit late, but:
"I am not able to see any output on the Serial monitor"
Note that this is to be expected: as the Getting Started Guide tells you, the ST-Link UART is disconnected from the target on the Nucleo board.
See my post of January 20, 2021 at 12:05 PM in this thread:
https://community.st.com/s/question/0D53W00000DHlVaSAL/i-want-to-get-pnucleolrwan2-gateway-source
2021-07-22 3:23 AM
Hello All,
I shared with you this post of @Andrew Neil (Community Member) , that contains the fixes proposed by JCOUP.
Hope this helps you !
Imen
2021-07-23 3:40 AM
Note that these fixes don't make any difference to the fact that the code does not - and is not intended to - give any output to a local terminal
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.