2025-02-10 5:41 PM
Hello,
I want to enable the secure connection key type as 'DEBUG' in STM32WB55 with my custom setup. The cube IDE does not allow this setting in the configuration of .ioc file. I followed this tutorial and added the following line in my code inside the definition of Ble_Hci_Gap_Gatt_Init() function, but it returns with error code 0x12 (Invalid HCI parameters). What am I missing here?
static const uint8_t SC_KEY_TYPE_DEBUG = 1;
static const uint8_t SC_KEY_TYPE_NORMAL = 0;
ret = aci_hal_write_config_data(0x35U, 1, (uint8_t*)&SC_KEY_TYPE_DEBUG);
if (ret != BLE_STATUS_SUCCESS)
{
APP_DBG_MSG(" Fail : aci_hal_write_config_data command - CONFIG_DATA_SC_KEY_TYPE_OFFSET, result: 0x%x \n", ret);
}
else
{
APP_DBG_MSG(" Success: aci_hal_write_config_data command - CONFIG_DATA_SC_KEY_TYPE_OFFSET\n");
}I am also following AN5270 for development, and the offset to set SC_KEY_TYPE seems to be correct.
This is what I am seeing when I run the code:
I made sure that CFG_SC_SUPPORT is set to 0x02 (supported and mandatory). What am I missing here?
Any help is appreciated!
Solved! Go to Solution.
2025-03-06 11:57 AM
Hi @STTwo-32 ,
Thanks for your reply. However, I was able to resolve the issue. Turns out, I was using a very old firmware version for the Bluetooth and was not aware that there is a newer version available. After updating to the latest version, the issue is now resolved.
2025-03-04 6:41 AM
Hello @tmk
I've sent this question to the concerned team (under internal ticket number 204530) and we will reach to you soon.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-03-06 11:57 AM
Hi @STTwo-32 ,
Thanks for your reply. However, I was able to resolve the issue. Turns out, I was using a very old firmware version for the Bluetooth and was not aware that there is a newer version available. After updating to the latest version, the issue is now resolved.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.