2022-05-19 10:28 PM
Hi, I'm having issues with RTC Alarm in Lora application. My RTC configuration works correctly when I run program configure only RTC. When I use Lora with RTC timer, the alarms not working. I use Sub-GHz Phy PingPong but I want Lora send and receive data while the alarms interrupt issue therefore I configure RTC in CUBEMX as free running BCD calendar mode. Does anyone have any tips what the issue might be? Thanks
2022-09-27 11:55 AM
Did you ever figure this out? I've been investigating trying to use the RTC in the LoRaWAN_EndNode application as well with no luck. Tested with the RTC_Calendar example and the RTC time (seconds, minutes, etc...) counts with no issues in that project so it doesn't seem to be hardware-related...
2022-09-27 9:29 PM
Hi,
The RTC Alarm A is used to configure Timer Server therefore don't use Alarm A for your purpose. Use Alarm B
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.