2023-01-11 1:49 AM
Hello,
we are working on new release of STM32WL "STM32Cube_FW_WL_V1.3.0". release which has introduced changes in RTC driver which we believe is fixed for the issue (RTC loosing time issue STMicroelectronics/STM32CubeH7#24 )
But, after running RTC overnight we have seen RTC issue is still persist in different manner this time RTC is increasing time
Test Start time : 17:55:56, UTC time 1670415956
Test End Time: 9:48:00, UTC time 1670473080, (57124 Seconds)
Difference of UTC time should be : 57124 (1670473080 - 1670415956)
But, From attached logs we can see Test End time is 9:48:00 and total seconds are 57135s837 (check last line in logs).
RTC had generated 57135s837 seconds instead of 57124 Seconds.
So, 57135 - 57124 = 11 Seconds are increased in actual time
Driver files are also attached for more details.
Can someone please explain how to fix this?
Solved! Go to Solution.
2023-01-12 11:20 PM
no, this crystal is running 193ppm too fast !
means: missing or wrong (too small) load capacitors.
check data sheet of the crystal and adjust caps to this.
read:
2023-01-11 5:12 AM
LSE oscillator may be designed improperly and run at higher than expected frequency, or it may be influenced by high-current adjacent signals.
Read AN2867.
JW
2023-01-12 1:33 PM
So it's slower by 193 ppm. That can easily be because of too much load capacitance for a crystal.
2023-01-12 11:20 PM
no, this crystal is running 193ppm too fast !
means: missing or wrong (too small) load capacitors.
check data sheet of the crystal and adjust caps to this.
read:
2023-04-04 2:04 AM
we have made changes in capacitance and now with release v1.3.0 module is providing correct time.
we have tested continuously 4 days and haven't seen any missing seconds on logs. thank you guys for the suggestion and quick support
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.