2022-07-04 10:35 PM
As of now, I work with the STM32WLE5JC controller. in that I need to interface CAN protocol for STM32WLE5JC board-to-board communication. For this is there any library available for this specific STM32WL controller and also which CAN module is suitable for interfacing with the STM32WL microcontroller. kindly guide me on this.
2022-07-04 11:11 PM
Dear @AA.21
There is a seeedstudio solution that you could use as reference
https://www.seeedstudio.com/LoRa-E5-CAN-FD-dev-kit-CANBUS-p-5398.html
2022-07-04 11:26 PM
I need to integrate STM32WL board to board communication by using external CAN bus module. So, Can you please suggest the suitable external CAN bus module (CAN controller +CAN transceiver integrated module) which provides UART interface to connect with STM32WL MCU?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.