2023-05-17 5:54 AM
Greetings,
I am working on the LoRaWAN Project and facing issues in updating RTC from a server/UART in LoRaWAN library.
My code is getting stuck while updating RTC, I am recieving time and from UART through user input.
RTC_TimeTypeDef set_time;
RTC_DateTypeDef set_date;
HAL_StatusTypeDef setTime_status;
HAL_StatusTypeDef setDate_status;
SysTime_t time;
set_date.Year = RxBuff->Buffer[1] - 12;
set_date.Month = RxBuff->Buffer[2];
set_date.Date = RxBuff->Buffer[3];
setDate_status = HAL_RTC_SetDate(&hrtc, &set_date, RTC_FORMAT_BIN);
set_time.Hours = RxBuff->Buffer[4];
set_time.Minutes = RxBuff->Buffer[5];
set_time.Seconds = RxBuff->Buffer[6];
if(set_time.Hours > 0x12){
set_time.TimeFormat = RTC_HOURFORMAT12_PM;
}
else{
set_time.TimeFormat = RTC_HOURFORMAT12_AM;
}
setTime_status = HAL_RTC_SetTime(&hrtc, &set_time, RTC_FORMAT_BIN);
Please Help me out from this. I found something on ST commnunity regarding same and one developer is setting RTC through void SysTimeSet( SysTime_t sysTime );
I am not able to understand this.
CurrentTaskId and TaskSet become 0 after updating RTC and code goes in NOTASKRUNNING mode and stuck in UTIL_SEQ_Idle( ) which returns nothing.
Please provide some code or another way to update the RTC in I-CUBE-LRWAN project. I want to use RTC for changing the interval time for LoRa uplink packets.
Regards,
Devesh Sehgal
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.