2023-01-26 8:11 AM
Hi Everybody!
New with STM32, i'm currently working on a project in order to combine black line detection with an AlphaBot and IA embedded with a TOF sensor, all of that with a Nucleo-WB55.
Actually I would like to add a Bluetooth function to be able to read informations about all the sensors.
The matter is : When I enable my RTC (mandatory with BLE), my timers (used to generate a PWM for the wheels motors) doesn't work : The right one doesn't move but the other one is at 100%.
Have you an idea of something to check?
Thank you!
2023-01-26 8:57 AM
Yes. Check your code. PWM timers are not related to RTC.
2023-02-01 8:43 AM
Hello @JDIRI.1 and welcome to ST Community,
Here is some suggestions:
It's possible that there could be issues in the RTC and timer configuration, so carefully review the code and the sensors to ensure that everything is set up and configured correctly.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.