2023-02-13 3:31 AM
Hi,
i have some pairing problems with a STM32WB board and a smartphone.
I have configured the STM32WB for working with the "Just Works" method (code attached).
static void Ble_Hci_Gap_Gatt_Init(){
uint8_t role;
uint16_t gap_service_handle, gap_dev_name_char_handle, gap_appearance_char_handle;
uint8_t *bd_addr;
uint16_t appearance[1] = { BLE_CFG_GAP_APPEARANCE };
hci_reset(); // Initialize HCI layer
// Write the BD Address
bd_addr = BleGetBdAddress();
aci_hal_write_config_data(CONFIG_DATA_PUBADDR_OFFSET, CONFIG_DATA_PUBADDR_LEN, (uint8_t*) bd_addr);
// Write Identity root key used to derive LTK and CSRK
aci_hal_write_config_data(CONFIG_DATA_IR_OFFSET, CONFIG_DATA_IR_LEN, (uint8_t*) BLE_CFG_IR_VALUE);
// Write Encryption root key used to derive LTK and CSRK
aci_hal_write_config_data(CONFIG_DATA_ER_OFFSET, CONFIG_DATA_ER_LEN, (uint8_t*) BLE_CFG_ER_VALUE);
// Set TX Power to max.
aci_hal_set_tx_power_level(1, CFG_TX_POWER);
// Initialize GATT interface
aci_gatt_init();
// Initialize GAP interface
role = GAP_PERIPHERAL_ROLE;
if (role > 0) {
const char *name = "IfSat";
aci_gap_init(role, PRIVACY_DISABLED, APPBLE_GAP_DEVICE_NAME_LENGTH, &gap_service_handle, &gap_dev_name_char_handle, &gap_appearance_char_handle);
if (aci_gatt_update_char_value(gap_service_handle, gap_dev_name_char_handle, 0, strlen(name), (uint8_t *) name))
BLE_DBG_SVCCTL_MSG("Device Name aci_gatt_update_char_value failed.\n");
}
if(aci_gatt_update_char_value(gap_service_handle, gap_appearance_char_handle, 0, 2, (uint8_t *)&appearance))
BLE_DBG_SVCCTL_MSG("Appearance aci_gatt_update_char_value failed.\n");
// Initialize Default PHY
hci_le_set_default_phy(0x00,0x02,0x02);
// Initialize IO capability
aci_gap_set_io_capability(CFG_IO_CAPABILITY); //3
aci_gap_set_authentication_requirement(CFG_BONDING_MODE, //1
CFG_MITM_PROTECTION, //0
CFG_SC_SUPPORT, //1
CFG_KEYPRESS_NOT_SUPPORTED, //0
CFG_ENCRYPTION_KEY_SIZE_MIN, //8
CFG_ENCRYPTION_KEY_SIZE_MAX, //16
CFG_USED_FIXED_PIN, // NOT USE FIXED PIN //1
111111,// FIXED PIN
PUBLIC_ADDR);
// Initialize whitelist
if (CFG_BONDING_MODE)
aci_gap_configure_whitelist();
}When the Smartphone connects, the board receives the connection complete event. In this event i ask for security update (line 20):
case HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE:
HAL_GPIO_WritePin(LED_BLUE_GPIO_Port, LED_BLUE_Pin, GPIO_PIN_SET);
connection_complete_event = (hci_le_connection_complete_event_rp0 *) meta_evt->data;
aci_gap_get_security_level(connection_complete_event->Connection_Handle,&sec_mode,&sec_level);
hci_le_read_phy(connection_complete_event->Connection_Handle,&TX_PHY,&RX_PHY);
printf("Client connected: %02X%02X%02X%02X%02X%02X SM=%d SL=%d TX=%d RX=%d\r\n", connection_complete_event->Peer_Address[0],
connection_complete_event->Peer_Address[1],
connection_complete_event->Peer_Address[2],
connection_complete_event->Peer_Address[3],
connection_complete_event->Peer_Address[4],
connection_complete_event->Peer_Address[5],
sec_mode,sec_level,TX_PHY,RX_PHY);
BleParams.ClientStatus = CLIENT_CONNECTED;
BleParams.connectionHandle = connection_complete_event->Connection_Handle;
TimerStop(BleParams.AdvTimeoutTimerId);
tBleStatus alfa = aci_gap_is_device_bonded(0,connection_complete_event->Peer_Address);
memcpy(BleParams.ClientAddress,connection_complete_event->Peer_Address,6);
printf("Client bonding status %02X\r\n",alfa);
printf("Pairing Request Sent\r\n");
aci_gap_slave_security_req(BleParams.connectionHandle);
P2PS_APP_ConnHandle_Not_evt_t pNotification = {EVT_LE_CONN_COMPLETE, BleParams.connectionHandle};
P2PS_APP_Notification(&pNotification);
break; /* HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE */So i send a pairing request to the initiator of the connection, this is made this way because in some smartphone OS it is not possible to send a pairing request, but only receive it.
This request sometimes does not work:
The number of successful cases are way less than the failures. Failures can happen in all of the following cases:
Which can be the problem? Is there a way to avoid it?
Thank you
2023-04-25 6:23 AM
Hello,
When you received the pairing complete event, what is the reason of the failure? Which smartphone application are you using?
Best Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.