2025-08-05 4:45 PM
The bottom line is the "wba" file stm32wbax.cfg is missing from openocd
Here are the details:
What I need is an openocd that works with the stm32wbax.cfg file.
I have found the file in https://github.com/openocd-org/openocd
However, that file does not work with openocd distributed by MorseMicro
And I built openocd from scratch and it also fail
Conclusion:
When you find the file stm32wbax.cfg, please make sure it works with openocd.
And please add LABELS to your GUI so I can file under STM32WBA or STM32WBA65
2025-09-16 9:03 AM
Hello @SWent.1
Could you please give more details about what is not working exactly and what is your test process.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-10-10 2:42 PM
I have the same issue, I can not get mainline top of tree regular openocd or ST fork of openocd to work with STM32WBA65.
For regular openocd:
clone: https://github.com/openocd-org/openocd.git
hash: 896738264e92b74a17250dab639999a2743d0b7c from 9/27/2025
For st fork
clone: https://github.com/STMicroelectronics/OpenOCD.git
hash: 0de861e21c12fd39fdce7b6296994d89eca6146f from 12/03/2024
When I run openocd with the following command-line it appears to work at first:
~/repos/openocd/src/openocd -s ~/repos/openocd/tcl -f interface/stlink.cfg -f target/stm32wbax.cfg
Open On-Chip Debugger 0.12.0+dev-02228-ge5888bda3 (2025-10-03-23:47)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Warn : DEPRECATED: auto-selecting transport "swd (dapdirect)". Use 'transport select swd' to suppress this message.
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V3J16M9 (API v3) VID:PID 0483:3754
Info : Target voltage: 3.267778
Info : Unable to match requested speed 500 kHz, using 200 kHz
Info : Unable to match requested speed 500 kHz, using 200 kHz
Info : clock speed 200 kHz
Info : SWD DPIDR 0x0be12477
Info : [stm32wbax.cpu] Cortex-M33 r0p4 processor detected
Info : [stm32wbax.cpu] target has 8 breakpoints, 4 watchpoints
Info : [stm32wbax.cpu] Examination succeed
Info : [stm32wbax.cpu] starting gdb server on 3333
Info : Listening on port 3333 for gdb connections
However as soon as I attach with gdb
Reading symbols from build/make.elf...
(gdb) target extended-remote localhost:3333
Remote debugging using localhost:3333
Remote communication error. Target disconnected.: Connection reset by peer.
(gdb)
And back in the openocd shell I now see
... continuing from previous ...
Info : Listening on port 3333 for gdb connections
Info : accepting 'gdb' connection on tcp/3333
Error: Failed to read memory at 0x40015800
Warn : Cannot identify target as an STM32C0/G0/G4/L4/L4+/L5/U0/U3/U5/WB/WL family device.
Error: auto_probe failed
Error: Connect failed. Consider setting up a gdb-attach event for the target to prepare target for GDB connect, or use 'gdb_memory_map disable'.
Error: attempted 'gdb' connection rejected
It doesn't contain stm32wbax.cfg so it fails.
If I try to use stm32wbx instead I get:
~/repos/openocd_st/src/openocd -s ~/repos/openocd_st/tcl -f interface/stlink.cfg -f target/stm32wbx.cfg
Open On-Chip Debugger 0.12.0-00033-g0de861e21 (2025-10-10-14:21) [https://github.com/STMicroelectronics/OpenOCD]
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : auto-selecting first available session transport "hla_swd". To override use 'transport select <transport>'.
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : clock speed 500 kHz
Info : STLINK V3J16M9 (API v3) VID:PID 0483:3754
Info : Target voltage: 3.267778
Warn : UNEXPECTED idcode: 0x0be12477
Error: expected 1 of 1: 0x6ba02477
^^^^ this would be expected of an unidentified ID.
2025-10-10 3:40 PM
Build a debug version, and stepping in, fundamentally the issue appears to be that even though I specified an stm32wbax.cfg, internally this ends up resulting in a flash "driver" object based on stm32l4.
Looking through those sources src/flash/nor/stm32l4x.c, I see mention of:
/* STM32WBxxx series for reference.
*
* RM0493 (STM32WBA52x)
* http://www.st.com/resource/en/reference_manual/dm00821869.pdf
*
* RM0434 (STM32WB55/WB35x)
* http://www.st.com/resource/en/reference_manual/dm00318631.pdf
*
* RM0471 (STM32WB50/WB30x)
* http://www.st.com/resource/en/reference_manual/dm00622834.pdf
*
* RM0473 (STM32WB15x)
* http://www.st.com/resource/en/reference_manual/dm00649196.pdf
*
* RM0478 (STM32WB10x)
* http://www.st.com/resource/en/reference_manual/dm00689203.pdf
*/
/* STM32WLxxx series for reference.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.