2021-09-14 8:04 AM
I just installed FUS 1.2 and BLE Stack Full firmware, I believe successfully based on the logs. I noticed that those sections of memory are not readable by CubeProgrammer. Are they encrypted once they're installed? Just kind of curious.
ST-LINK/SWD connection, Nucleo-WB55RG
Solved! Go to Solution.
2021-09-20 8:05 AM
Once the wireless stack installed at the top of the Flash memory, this area is protected from any read access for security reason as this code is not encrypted any more. So It cannot be accessed by CubeProgrammer either. This protected zone is materialized by the SFSA option byte pointing on the first sector of this secure zone which is in fact containing the code to be executed by the M0+ core.
2021-09-20 8:05 AM
Once the wireless stack installed at the top of the Flash memory, this area is protected from any read access for security reason as this code is not encrypted any more. So It cannot be accessed by CubeProgrammer either. This protected zone is materialized by the SFSA option byte pointing on the first sector of this secure zone which is in fact containing the code to be executed by the M0+ core.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.