2020-01-29 2:27 AM
Hey there,
bringing my custom STM32WB board up, I encountered a problem with the RTC initialization. I recently updated CubeMX to 5.5.0 and I don't know, if my problem comes with the update, but with the older versions I didn't have these type of errors. Anyways, I set up the RTC, which at first only worked after a power down reset. Resetting per reset pin brought me trouble with the RTC_EnterInitMode() function. There was only a Timeout error. At first I thought of a hardware problem, but after reconsidering the example brought by the firmware, I saw major differences in the stm32wbxx_hal_msp.c file. The CubeMX generated file lacked the following code
/* USER CODE BEGIN PV */
static uint32_t RtcClockSource
#ifdef RTC_CLOCK_SOURCE_LSE
= RCC_RTCCLKSOURCE_LSE;
#elif defined (RTC_CLOCK_SOURCE_LSI)
= RCC_RTCCLKSOURCE_LSI;
#endif
/* USER CODE END PV */
.
.
.
/* USER CODE BEGIN RTC_MspInit 0 */
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
/* Enables the PWR Clock and Enables access to the backup domain */
/* To change the source clock of the RTC feature (LSE, LSI), You have to:
- Enable the power clock using __HAL_RCC_PWR_CLK_ENABLE()
- Enable write access using HAL_PWR_EnableBkUpAccess() function before to
configure the RTC clock source (to be done once after reset).
- Reset the Back up Domain using __HAL_RCC_BACKUPRESET_FORCE() and
__HAL_RCC_BACKUPRESET_RELEASE().
- Configure the needed RTC clock source */
HAL_PWR_EnableBkUpAccess();
/*##-2- Get RTC clock configuration #########################################*/
HAL_RCCEx_GetPeriphCLKConfig(&PeriphClkInitStruct);
/*In case of RTC clock already enable, make sur it's the good one */
if (PeriphClkInitStruct.RTCClockSelection == RtcClockSource)
{
/* Do nothing */
}
else
{
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_RTC;
/* If selected source was previously the opposite source clock, first select none*/
if (PeriphClkInitStruct.RTCClockSelection != RCC_RTCCLKSOURCE_NONE)
{
PeriphClkInitStruct.RTCClockSelection = RCC_RTCCLKSOURCE_NONE;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
}
/* Configure LSE/LSI as RTC clock source */
#ifdef RTC_CLOCK_SOURCE_LSE
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSI1 | RCC_OSCILLATORTYPE_LSE;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
RCC_OscInitStruct.LSEState = RCC_LSE_ON;
RCC_OscInitStruct.LSIState = RCC_LSI_OFF;
#elif defined (RTC_CLOCK_SOURCE_LSI)
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSI1 | RCC_OSCILLATORTYPE_LSE;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
RCC_OscInitStruct.LSIState = RCC_LSI_ON;
RCC_OscInitStruct.LSEState = RCC_LSE_OFF;
#else
#error Please select the RTC Clock source inside the main.h file
#endif /*RTC_CLOCK_SOURCE_LSE*/
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
PeriphClkInitStruct.RTCClockSelection = RtcClockSource;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
}
/* Enable RTC peripheral Clocks */
/* Enable RTC APB clock */
__HAL_RCC_RTCAPB_CLK_ENABLE();
/* USER CODE END RTC_MspInit 0 */After inserting it in my project, it worked. Did I forgot something some configuration in CubeMX or is it a bug?
Thanks in advance :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.