2021-06-14 5:01 AM
Hi,
I want to implement BLE read property.
I found Blood pressure example but not able to execute and understand it properly.
Thanks.
2021-06-15 10:07 AM
The Heart Rate project includes a characteristic with the READ property.
#if (BLE_CFG_HRS_BODY_SENSOR_LOCATION_CHAR != 0)
/**
* Add Body Sensor Location Characteristic
*/
uuid = SENSOR_LOCATION_UUID;
hciCmdResult = aci_gatt_add_char(HRS_Context.HeartRateSvcHdle,
UUID_TYPE_16,
(Char_UUID_t *) &uuid ,
1, /* bytes */
CHAR_PROP_READ,
ATTR_PERMISSION_NONE,
GATT_DONT_NOTIFY_EVENTS, /* gattEvtMask */
10, /* encryKeySize */
0, /* isVariable: 0 */
&(HRS_Context.BodySensorLocationCharHdle));
The Blood Pressure project too.
#if (BLE_CFG_BLS_SUPPORTED_FEATURES == 1)
/**
* Add Blood Pressure supported features Characteristic
*/
uuid = BLOOD_PRESSURE_FEATURE_CHAR_UUID;
hciCmdResult = aci_gatt_add_char(BLS_Context.SvcHdle,
UUID_TYPE_16,
(Char_UUID_t *) &uuid ,
2,
CHAR_PROP_READ,
ATTR_PERMISSION_NONE,
GATT_DONT_NOTIFY_EVENTS, /* gattEvtMask */
10, /* encryKeySize */
CHAR_VALUE_LEN_CONSTANT, /* isVariable */
&(BLS_Context.FeatureCharHdle));
if (hciCmdResult == BLE_STATUS_SUCCESS)
{
BLE_DBG_BLS_MSG("BLS Pressure Feature Characteristic Added Successfully %04X \n",
BLS_Context.FeatureCharHdle);
}
else
{
BLE_DBG_BLS_MSG ("FAILED to add BLS Pressure Feature Characteristic, Error: %02X !!\n",
hciCmdResult);
}
#endif
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.