2022-06-28 7:14 AM
### Flashing Target ###
Open On-Chip Debugger 0.11.0+dev-00748-ga70bab9e5 (2022-06-28-14:36)
Licensed under GNU GPL v2
For bug reports, read
hla_swd
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
Info : DEPRECATED target event trace-config; use TPIU events {pre,post}-{enable,disable}
/home/thomas/myRIOT/boards/common/stm32/dist/stm32wl.cfg:4: Error: can't read "_TARGETNAME": no such variable
in procedure 'script'
at file "embedded:startup.tcl", line 26
at file "/home/thomas/myRIOT/boards/common/stm32/dist/stm32wl.cfg", line 4
make: *** [/home/thomas/myRIOT/examples/hello-world-wl/../../Makefile.include:837: flash] Error 1
if i try to flash the .bin with the stlink-flash i receive the following message:
st-flash write hello-world.bin 0x8000000
st-flash 1.6.0
2022-06-28T15:42:25 WARN usb.c: Couldn't find any ST-Link/V2 devices
As far as I know the Nucleo-WL55 uses a STLink-V3 is this the cause of my problem?
How to fix this?
lsusb
responses with
Bus 003 Device 005: ID 0483:374e STMicroelectronics STLINK-V3
2022-06-28 7:58 AM
Compare cfg files or use Windows...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.