2025-05-11 2:15 PM
I am working on STM32WLE5CCU6 mcu and try to erase the flash. But always giving me the error status as 0xFFFFFFFF.
whatever address we provide , the errorStatus is always 0xFFFFFFFF
memAddress = FLASH_BASE + (110*FLASH_PAGE_SIZE); //0x08037000
uint32_t eraseFlash(uint32_t memAddress)
{
uint32_t errorStatus = 0;
FLASH_EraseInitTypeDef flashEraseStruct = {0};
flashEraseStruct.TypeErase = FLASH_TYPEERASE_PAGES;
flashEraseStruct.Page = (MemAddress - FLASH_BASE) / FLASH_PAGE_SIZE;
flashEraseStruct.NbPages = 1;
HAL_FLASH_Unlock();
HAL_FLASHEx_Erase(&flashEraseStruct, &errorStatus);
HAL_FLASH_Lock();
if(errorStatus == 0xFFFFFFFF)rtn = 0;
printf("errorStatus : %.X\r\n",errorStatus);
return rtn;
}
can anyone help me with this ?
Solved! Go to Solution.
2025-05-11 4:22 PM - edited 2025-05-11 4:22 PM
Check the return value of HAL_FLASHEx_Erase to assess whether or not it succeeded. It will return HAL_OK on success. The error status variable is always initialized to 0xFFFFFFFF for page erases and does not indicate an error.
2025-05-11 4:22 PM - edited 2025-05-11 4:22 PM
Check the return value of HAL_FLASHEx_Erase to assess whether or not it succeeded. It will return HAL_OK on success. The error status variable is always initialized to 0xFFFFFFFF for page erases and does not indicate an error.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.