2025-05-15 8:06 AM - edited 2025-05-16 12:17 AM
2025-05-16 1:36 AM
Hello @OGarc.1
Thank you so much for posting on the ST Community.
this is the original post:
Hi again Annis,
It seems that the option to save the zigbee connection in our end node coordinator for a maximum time of 11 days, is not enough and I would like to know if there is an option to instead of modifying the time ZB_NWK_CONST_ENDDEV_TIMEOUT_MAX, I could disable this register so that the connection in the coordinator lasts forever.
Is it possible to disable this option?
stEntry.interval = ZB_NWK_CONST_ENDDEV_TIMEOUT_MAX;
Thanks in advance.
Best Regards,
For the future, please avoid deleting the content of your post and if your issue is solved, you can post the solution on the community to help others on it.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.