2025-11-19 2:42 AM
Hello,
I am using the Nucleo STM32WB55 board and noticed that when I press the user button, the interrupt service routine (ISR) is triggered only after about 3.5–4 seconds. This delay occurs even before reaching the callback function — the ISR itself is reached late.
I have not initialized or configured any BLE stack functionality; this is just a basic GPIO interrupt setup. I have also used other Nucleo boards and never experienced this kind of delay.
Has anyone else encountered this issue or found a solution?
Thanks,
Shreyas
Solved! Go to Solution.
2025-11-19 3:15 AM
Check if the pull-up resistor is enabled on button input port line.
2025-11-19 3:15 AM
Check if the pull-up resistor is enabled on button input port line.
2025-11-19 3:34 AM
Enabling the pull-up on the button input fixed the issue. The interrupt now fires immediately.
Thanks
Shreyas
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.