2024-03-05 12:32 AM
Hello,
Currently, I am working with custom clusters, and I have a requirement related to transmitting and receiving the maximum number of attributes.
To illustrate, consider a cluster with three attributes:
Data Set - SET_0
-------------------
Valid_data_set (True/False),
Attribute_A (<Attr_A_Data>) and
Attribute_B (<Attr_B_Data>)
which I interpret as SET_0
Now, let's introduce three more data sets, SET_1 and SET_2.
In this setup, I have Zigbee Endpoints acting as servers, and the coordinator acts as the client, requesting these sets.
Question: I need to dynamically send data over these data sets. Specifically, I want to send data only if the Valid_data_set attribute of SET_0 is true. Similarly, I need to check and send in a single packet.
For example, if I have four sets with Valid_data_set attribute set to True out of a total of six sets, I want to send only those four sets of data to the coordinator upon a Zigbee request.
Suggestions and any other references are greatly appreciated.
--
Thanks,
Naani Ch
2024-03-06 12:36 PM
Hi All,
This question has been routed to our Online Support Center for direct support.
Regards,
Jake
ST Support
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.