cancel
Showing results for 
Search instead for 
Did you mean: 

Bluenrg-2, Calling BTLE_StackTick() in ISR of a periodic timer.

_Abdelrahman_
Associate

Hi,

I use BlueNRG-2 in my project and the archive library libbluenrg1_stack.a.
I use Project for BLE always connected and other operations like saving data in Flash; I need to call BTLE_StackTick() periodically.
I faced problems in the project, like Disconnection reason 0x22 and latency to raise Vtimer cb, and I think it's related to the calling of the BTLE_StackTick().

Can I call BTLE_StackTick() in the ISR of a periodic timer instead of calling it from the main while loop?
I need to make sure that I call it periodically without any latency. Is it a valid option to call it from ISR?
I tried to use it inside ISR, but I faced many disconnections, reason 0x22, 0x8, and many system resets.
How should I handle it?

Regards,

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.