STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 303 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4120 Views
  • 0 replies
  • 3 kudos

Resolved! Connection interval update using BLE_SVC_L2CAP_Conn_Update

Hi. I'm currently implementing an application for test purposes on the STM32WB Nucleo Demoboard. So far I'm very pleased with the experience of adding new services and transvering data. However, to save some energy I want to change the connection int...

Need help related freeRTOS timing mechanism implementation, on BLE P2P Server project, running on STM32WB, instead of existing UTIL_SEQ_Run(~0) timing mechanism

Hello,I made several modifications to the STM32WB HandsOn_3 example (based on p2p-server project located at c:\STM32WB_workshop\HandsOns\HansdsOn_3) and succeeded to communicate with my mobile application - all OK =) However the above working soluti...

I have two different STM32WB55 Nucleo boards in a state where the debugger cannot connect to the target. Is there an errata I'm missing?

I am using the ST32CubeIDE and the imported HeartRate project from the STM32CubeWB package. For both boards the project compiles and is loaded into the board, and then the boards just stop working during debugging. I am not probing the boards or t...

Resolved! USB dongle CLI firmware doesn't work

I couldn't get the CLI application running on the P-NUCLEO-WB55.USBDongle. I updated the FUS firmware according to ../STM32WB_Copro_Wireless_Binaries/Release_Notes.html and installed the stm32wb5x_Thread_FTD_fw.bin on CPU2. The FUS update exited with...

TWirt.15 by Associate II
  • 4419 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.