NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I'm using a custom board with a STM32WB50CG part. When I send this:0x10 0xFC 0x52 0x00 (FUS_GET_STATE) or any command for that matter, I always get this back:0x11 0x0E 0x04 0xFF 0xFE 0x00 0xFE 0x00I've tried this while running the bootloader code as ...
I have Lora module with STM32L052C8T6 mcu. I like to send short massages every minute or two. I sent data with success alredy, but my device will be battery powered so I need very power efficient approach. I figured out that stop mode will be best su...
Is there something similar like X-CUBE-BLE2 (which is for BlueNRG-2) for STM32WB with transparent mode firmware? We want to use STM32WB as a network coprocessor and control it with external STM32 MCU via UART. It's pretty clear what needs to be don...
HiIm working on custom template from STM32WB Workshop HandsOn_3 with template BLE server. I've tried to add more custom characteristics (notify with variable values) to my service. Ive modified the code to the moment that I see them on the Client BLE...
Hi,Is there any example/Demo available which represent complete BLE security. i.e Paring using numeric comparison method and also only authorized person can read or write BLE characteristics.How we can implement such kind of security in stm32wb55. Pl...
Hey Guys,I have a problem with my STM32WB55CC. For the certification of my product I have to set the advertising channel to a fixed one (37, 38, 39). The command I try to use is the following:volatile uint8_t ret; ret = hci_le_set_advertising_paramet...
Using DFU. I repeatdly try to flash the dongle, it almost always fails and when it seems to start erasing prior to writing it ends up with :$ ./STM32_Programmer_CLI -c port=usb1 -d /tmp/BLE_p2pServer_reference.hex -------------------------------...
Hello,I am a newbie and trying to get debugging on my STM32WB55 USB Dongle Board to work.I have LPUART1 and USART1 set up, but don't understand what else is required to set up?Is there any example project for the USB Dongle Board using the USB conne...
Hi,where can i find AN5500: ZSDK API for ZigBee® on STM32WB Series, referenced in AN5492 to be available on www.st.com?Regards, Rainer
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.