STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

RX Interrupt pin issue - CMWX1ZZABZ-078

Hello everybody,my project is composed by a RX board and one/many TX boards (max 3). Every board uses CMWX1ZZABZ-078 module.The TX boards transmit asynchronously to the RX board a payload of 32 bytes (they are temperature IR sensors which communicate...

AComa.170 by Associate II
  • 1197 Views
  • 0 replies
  • 0 kudos

Resolved! Help with STM32WB External Flash Loader using Quad SPI memory

Hi,I am writing an external flash loader for the STM32WB55RGVx using a Macronix 64Mbit QSPI NOR Flash (MX25R6435F).I have had some success following the "MOOC - External QSPI loader how to" youtube video series by ST and the example code for memory m...

SThon.1 by Associate II
  • 10475 Views
  • 6 replies
  • 0 kudos

Resolved! PWM Frequency wrong

HiI'm trying to generate a 64 kHz PWM with 50% dutycycle. I've configured the SYSCLK to use the HSE in combination with the PLL resulting in 64 MHz. Since I'm using TIM1, which is on APB2, I've configured the APB2 timer clock also to 64 MHz. However,...

0693W000003RGVuQAO.png
secures by Associate
  • 2026 Views
  • 3 replies
  • 0 kudos

Fatal error: no input files

Hey guys,I am new to stm32 microcontrollers.I am using CubeMX to generate my projects. I already accomplished to start a new project with the board STM32WB55 Nucleo and to program the timer / leds etc.However, if I try to build an example project fro...

RWeil.2 by Associate III
  • 1697 Views
  • 1 replies
  • 0 kudos

how to connected P-NUCLEO-LRWAN2 to pc server.

I will use P-NUCLEO-LRWAN2.Lora device is a custom board by made me.I want to use P-NUCLEO-LRWAN2 gateway.so, I saw user manual. but the user manual explains just TTC and Loriot. I really want to function is Data come from Lora device send to pc serv...

Jlim.1 by Associate II
  • 733 Views
  • 1 replies
  • 0 kudos

STM32WB p-nucleo-wb55 fus upgrade

Hi! I have p-nucleo-wb55 board. I watch very strange behavior: all ok, when I load precompiled demo from st.com. But when I compile hex from example sources(ble_p2pserver application), board not working. Green LED lighten 1 minutes, but not blinked, ...

IIvan.10 by Associate
  • 1355 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.