NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I would like to create a ZigBee application on STM32WB55 controller for CubeIDE. Unfortunately there are no .IOC example files for ZigBee. What components do I need to select in CubeMX to be able to use ZigBee? Should I enable BLE or THREAD (WPAN). ...
HiHas anyone tried connecting the STM32WB and the Serial Bluetooth Terminal application ? https://play.google.com/store/apps/details?id=de.kai_morich.serial_bluetooth_terminal&hl=sk does anyone know how to set up Bluetooth in STM32CubeMX ? or is ther...
I would like to communicate wirelessly between the stm32 nucleo f446reboards with ai-thinker's ra-02 sx1278 module. However, there is no relevant code for the module that i am trying to use, so I don't know how to start it. So can I get the relevant ...
Hi,for my application i need to connect from 8 to 16 BLE devices (STM32WB sensor boards) to a LTE gateway (always a STM32WB board). Since actually the maximum connectable devices in master mode are 5, I found not ideal the solution to switch device t...
Helloi'm an electronic engineer and i'm working on LORA project using the i-cube-lrwan expansion package. An expansion package by definition must include .ioc file for STM32CubeMX but the LORA expansion package doesn't include this file!!! why?i work...
Hello,I'm trying to update the firmware of my I-NUCLEO-LRWAN1. But before that, I would like to backup the firmware. I'm trying to use the sm42_fw_update_tool found here:https://github.com/USIWP1Module/USI_I-NUCLEO-LRWAN1I got the same error seen her...
Hello,I'm working on the I-NUCLEO-LRWAN1 LoRa expension board.I succesfully build an application PingPong for this board. It is working fine. (Two module communicating!)To understand better what is done, I would like to check the AT commands send to ...
helloI am flashing my BLE module via STM32_Programmer_CLI.it takes about 2 minutes (!) to flash the board.the flashing includes 4 applications:stm32wb5x_FUS_fw.binstm32wb5x_ble_stack_fw.binMy_Bootloader.binMy_applicaiton.binthis is the command line i...
hi.. i am trying to use ble_p2pserver example in order to advertise and connect. I want the device to be in advertising mode still it connects to any client. so i have not registered event for ADV_Cancel. unfortunately, Advertising event is getting s...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.