STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

USART fifo mode STM32WB

Hello, I'm using STM32WB55 for my application.My code is divided in 2 parts, bootloader and application.I configured the bootloader using USART 1 with FIFO mode disabled. In the application I initialize again the USART 1 using the FIFO mode (enabled)...

Bluetooth does not work at stm32wb35cc

I followed the example by viewing the file "03-STM32WB-WS__How_to_add_BLE_functionality_V2.2.pdf" in stm32wb workshops. ​The stm32wb55rg evk succeeded in Bluetooth communication with this example of the pdf file.Now I applied my custom board, stm32w...

Jlim.1 by Associate II
  • 952 Views
  • 1 replies
  • 0 kudos

Is I-CUBE-LRWAN has LBT ?

I used I-CUBE-LRWAN develop my sensor node. The problem is when a network have sensor node more than 15 node, sometime they can't transimit data to gateway. I found a recomend for other device that mcu have to eanble LBT to avoid the collision. Pleas...

stm32 to stm32 download

If the stm32 mcu is connected as shown in the figure below, is there a way to download fw image from the master stm32(STM32WB35) mcu to the slave stm32(STM32L0) mcu?​

0693W000007BEluQAG.png
Jlim.1 by Associate II
  • 2311 Views
  • 5 replies
  • 0 kudos

Small rant on the wl55jc1 board..

Just got two of the WL55JC1 boards today, and while working just fine transmitting data, the usb connectors are really bad. Can barely touch the usb without it disconnecting and resetting the board..I will try and resolder the connector and see if th...

TResell by Associate II
  • 1614 Views
  • 3 replies
  • 0 kudos

Dificulties with the I-NUCLEO-LRWAN1 aka WM-SG-SM-42

Im trying to use the STM32 Nucleo Pack LoRa HF band sensor and gateway, and im trying to program the I-NUCLEO-LRWAN with the firmware, but im getting no responde from the shield. I did a little bit of research and found out about the firmware update ...

CSilv.1 by Associate
  • 1224 Views
  • 1 replies
  • 0 kudos

Creating BSP for Custom STM32 Board with I-CUBE-LRWAN

I have a custom board with STM32 microcontroller and SX1261 Radio Module. I am familiar with I-CUBE-LRWAN from ST Micro. I used the I-CUBE-LRWAN Package in a Nucleo Board and it is working fine. I understand that I need to create a new BSP if using c...

BSada.1 by Associate
  • 1404 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.