NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi, I'm working on the Lora project. I have a STM32F767ZI board and an I-NUCLEO-LRWAN1 module. As I understood from the manual to the module. The module is programmed using AT commands via UART. I set up USART3 on my board to communicate with a PC th...
Good day,So the STM32WB microcontrollers have all been tested and qualified with the Bluetooth Special Interest Group (SIG). (Search for "STM32WB" on here: https://launchstudio.bluetooth.com/Listings/Search).However, the new STM32WB5MMG module does n...
Hello,I am a beginner with ble. I have worked with other stm boards in the past. I need help with the STM32WB baord.I used cube mx to generate the start up code. Enabled rf, rtc and everything.Enabled custom template in server modeadded a service and...
Hello, community!I need to design a device that can work from a single-cell Li-Ion battery (~500mAh) of at least 1.5 years. STM32WB55 has SMPS which can increase consumption efficiency, the maximum input voltage for SMPS is 3.6V but the battery volta...
After the Return instruction, the Cortex M goes into Hardflault.I use the STM32CubeIder 1.5.1.. It uses sequencer.c. I attach two screen prints:The:void HAL_GPIO_EXTI_Callback, where there is a breakpointand that of the fault analyzer:
Hello Geeks!I'm playing with STM32WB.Actually, I'm using in one of our product as an SOCI'm using the Former version of the Cube packages, i guess "1.7.x"As we all know, the former version of the Cube packages was unstable and almost impossible to pl...
Board: Nucleo-WB55I'm attempting to continuously interrupt when data is received via UART. The program is able to receive data when it is sent without fail, however the Rx interrupt is triggered when new data is not sent. I implement the following lo...
Hello We are using STM32WB55xx STM32WB35xx Nucleo board with STM Ble stack. We want to transfer data around 2Mbytes after connection.After connection, we are only able to transfer around 100Kbytes of data after that connection is getting lost.What i...
Is it possible to pasively scan on this kit? Example with active scan works(BLE_p2pRouteur from git repo).Just to understand what I need - chip have to to advertise data while pasively scan all beacons around.Moreover in document PM0271 Rev 1, July 2...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.