NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hey all,I am trying to use the STM32WB55RG Nucleo board and for the application, I would have to use the board with the coin battery power supply (There is a coin battery slot for CR2032 battery). However, I could not see much information on how to c...
Are additional external circuit components needed to reliably connect USB voltage to an ADC input, besides a voltage divider that brings 5V down to 3.3V?
Hello,I've confirmed my registration on feb 25th, but today i got an email stating my registration can't be confirmed. Is this an error?
Hello,I just received an email from ST; I registered for the 30 March workshop but due to reached capacity my registration was not confirmed. I would like to ask if there is the possibility to join the workshop on another day.Thank youAlessandro
I try to create end_node project for stm32wl5cc uC, but for unkonw reason to me it is impossible "End_Node" option is inaccessible (grey).In LoRaWAN_End_Node example it is available.Ho to do this in Cube Ide.When I try to import project from NUCLEO-W...
It is possible to use the ISE 1.6.0 instead of 1.5.1?
When a P2P server is advertising I am able to see the raw data values of the advertisement as well as the explained details using mobile app.(nRQ connect) Here I need to find exact same things using STM32WB as a client. I am struggling to find a way ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.