NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I want to know whether any option bytes should be set before doing global erase for STM32wb chip. After the initial 0x44 and 0xBB, the device doesnt respond to global erase command (0xFFFF).
Using an STM32WB5. Using the ADC for some slow periodic measurements. Its working fine. Then added in STOP0:LL_PWR_SetPowerMode( LL_PWR_MODE_STOP0 )The ADC does not recovered on STOP exit. Value of:hadc->Instance->ISRis causing a hang in:HAL_ADC_Poll...
I'm using the STACK "stm32wb5x_Mac_802_15_4_fw.bin"on the STM32WB55 and in principle it works correctly.The problem is that after a few hours and after having been working correctly it seems that the cortex-M0 does not answer to the cortex M4 and I g...
In the wiki ( https://wiki.st.com/stm32mcu/wiki/Connectivity:STM32WB_FUS ), it is said:Interfaces that can be used to communicate with FUS are:System bootloader (USB DFU and USART): provides ready-to-use commandsSWD (FUS_Opeartor): provided by ST ins...
Hi everybody,I want to design a custom PB for the STM32WB10 with the PCB antenna design from AN5129. As described in the document there is a keep out area for the antenna where no GND plane should be placed. My question about this:If I keep this spac...
I am currently working with the STM32WBMMG discovery board.Initially, I powered the board through USB STLink(CN11), and was able to download the p2pserver program. Everything works perfectly. But if I power this board using an external power 3.3V as...
Hi, I am using VREF to calculating VDD. VDD = 3.3V but VREF = 3.0V. What wrong? (I use __LL_ADC_CALC_VREFANALOG_VOLTAGE() macro helper to calculate Vref). Does anyone have any tips what the issue might be? Thank.
Hello ST,During the provisioning in mesh network a node address assigned by PROVISIONER. which is going to be stored in LPN node memory. -----------------Debug Trace-----------BLEMesh_PbAdvLinkOpenCb - PB-ADV Link opened successfullyBLEMesh_PvnrDataI...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.