STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Connection of paired client not working

Hello,Setup:STM32WB,Wireless Firmware version 1.14.1Wireless Firmware build 1FUS version 1.1.0Working on a custom boardPhone Xiaomi MI A2 Android 10My issue is that my custom device (server) don't accept connection with a phone (client) that is alrea...

HSAADI by Associate III
  • 1135 Views
  • 0 replies
  • 1 kudos

Resolved! Ble application gets stuck when terminating scanning

I have a program that builds upon the p2p example.The scanner starts when I press a button withaci_gap_start_general_connection_establish_proc(HCI_SCAN_TYPE_ACTIVE, LE_Scan_Interval, LE_Scan_Window, PUBLIC_ADDR,0x00, 0);If the button is held for 5 se...

WRosé.1 by Associate II
  • 1327 Views
  • 2 replies
  • 1 kudos

Basic steps to get OPENTHREAD up and running

Has anyone got a simple example of the steps needed to get THREAD working? I have followed the application notes and cant get things working :( I have got the STM32WB55 nucleo board running with OpenThread FTD CLI example code nicely, but would like ...

RPars.1 by Associate
  • 1454 Views
  • 1 replies
  • 0 kudos

Test Report and Declaration of Conformity

Dear all,I develop a LoRa device that is built around STM32WLE5CCU6. In order to certify the product with CE marking from a notified body, I need to have the test reports and the declaration of conformity for STM32WLE5CCU6.Does anyone know where I ca...

STM32WL55 subghz radio low level hardware init.

Hi, im currently working on a project (STM32WL55) where i need to send data via LoRa. I plan to use the SubGHz HAL driver as it seems pretty low level and provides easy usage of the internal subghz spi.While researching, i found AN5406 where it says ...

D.Heink by Associate III
  • 4723 Views
  • 5 replies
  • 1 kudos

STM32WB Firmware OTA stalls for some images

Hi,I am using a STM32WB55RG MCU and I flashed a custom BLE_Ota application on it that uses the HSE clock instead of the default LSE and where the user app starts at 0x10000 instead of the default 0x7000.I am using FUS v1.2.0 and BLE Stack 1.13.0.Usin...

apous.1 by Associate II
  • 1144 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.