STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! stm32wb how to use the full SRAM2b

We are using the ST32WB without making use of the BLE feature.But we run into RAM issues and need more RAM. How can we "non-secure" the SRAM2Bb part?SRAM2a is currently already non-secure.Tried to do it from the CubeProgrammer, but got the error:Erro...

Question about sx1262 example

Hi stm, ​We are currently reviewing the lora function based on sx1262 semteck chip.​I have NUCLEO-L476RG and NUCLEO-L073RZ ref board. It also has an sx1262 Evaluation board that can be attached to the ref board. ​The NUCLEO-L476RG board has a flash o...

Need I2C Code base with 1 Fast Mode

Hi Team,We are using the I2C Bus to read the Eeprom Data. We configured with 100Khz speed with DMA to transfer the data.After initialization of I2C and DMA it is working fine and able to Read and write the data with different speeds.If we read the da...

Resolved! How can enable the SYSCFG in STM32WB55RGV6

Hi,I want to enable the SYSCGF in STM32WB55RGV6 , but when ı look the reference manuel; it says that SYSCFG is on the APB2 bus however when look the APB2ENR register there is nothing about SYSCFG . What should ı do to enable SYSCFG?

MOB1 by Associate II
  • 2300 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.