NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
This is coming from someone with very limited experience with BLE, so be patient in your response.I have a requirement for a device that will operate as a GATT Server emulating a UART to an external device (IOS or Android). On input from the user, th...
Hi,I need to implement the following behavior on a STM32WB55.Upon a command, device must advertise in 2 different modes:Just works. No bonding, connection is accepted without any authentication requirements. All characteristics can be read and writte...
Hi,I'm having an issue with the WBA6_LinkLayer_BLE_Basic_lib.a library on zephyr.The library is found in zephyrproject/modules/hal/stm32/zephyr/blobs/stm32wba/lib directory in zephyr 4.2 (tag v4.2.0 in https://github.com/zephyrproject-rtos/zephyr/tag...
Hi,I got a NUCLEO-WB55RG board and was trying to program it as a HID device. I have configured the STM32CubeIDE and have uploaded the code to the board. Yet, when I tried connecting the User USB, it unfortunately didn't work. My computer did not reco...
Hello,I have created two BIS channels eng and esp, under BIG main group by assigning bis[0] and bis[1] and given left and right channel as the input. At the receiver side, the first channel [0] will perfectly get connect and displays "synced with som...
The parameters for the AT+TCONF are shown differently in your example to where you show the breakdown of the individual paramters.In your example you show the <cr. parameter on the command line as 4/5 868000000:14:125:12:4/5:0:0:1:255:0:0:0where in...
背景描述:1.我现在使用的是:STM32Cube_FW_WB0_V1.4.0\STM32Cube_FW_WB0_V1.4.0\Projects\NUCLEO-WB09KE\Applications\BLE\BLE_DataThroughput_Server中BLE_DataThroughput_Server例程2现在使用的是STM32CUBE6.16进行配置需要帮助:1BLE_DataThroughput_Server例程中用到了UART1RX和UART1TX,我的项目中这两个引脚另有他用,但是...
Dear all,with the latest update of STM32Cube_FW_WBA_V1.8.0, the BLE_p2pServer_TZ example no longer works. The following error occurs during compilation:make: *** No rule to make target 'C:/0_ST_abc/Example/Projects/Common/WPAN/Interfaces/app_bsp.c', ...
Hello Community,I have been working on a BLE project in which the server needs to send notification of a characteristics that is up to 512 bytes long. As in previous CubeMX versions (6.12 and before), I was expecting CubeMX to generate the function C...
I'm having trouble changing the linker files to take 20 kB of flash from CM0+ for CM4's use on a STM32WL5. Is this possible?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.