NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Using the NUCLEO board with STM32WB.Device is currently configured as server to act as a peripheral. (one of the examples)I am interested in connecting it to multiple central.Is it possible?Any example will be great.
I developed a software to collect LC sensor measurement and upload the data to TTN via LoRaWAN. The software is working well in NUCLEO-WL55JC1 but failed to run on my own board with STM32WLE5 MCU. My program is written for single core only so it shou...
We developed our software in our STM32WLE5 board for LoRaWAN applications. It is working well to connect the TTN with OTAA in the NUCLEO-WL55JC1. When we migrated the software to our board with modification of the RF switch control GPIO pins, the sof...
Hi,we've been testing STOP2 modes and faced random core2 crashes.We use radio stack 1.15.0 LightCrash data at 0x20030000: 0x1170fd0f 0x00000000 0x00000939 0x2003fa20Any ideas?
Hello, Thank you for any feedback on this issue.i am using the Freertos Heartrate example shipped with the SDK as a starting point.i have noticed that the float type is not getting printed in the debug messages, so i enabled the "use float with print...
Hi,I am currently using the package version 1.6.0 on a STM32WB55.When i configure the STM32WB55 on CubeIDE, it seems that select RTOS with CMSIS_V2 and the BLE Application Type "Server profile" configuration is possible, in fact the code is generated...
I made a PCB board with STM32WB5MMG, which receives the data of max30112 through external falling edge interrupt and sends it through BLE notify. However, once I add the execution task UTIL_SEQ_SetTask(1<<CFG_TASK_SPO2_EVT_ID,CFG_SCH_PRIO_0); in HAL_...
Hi, I am working on STM32WB5MMG controller and now I want to see bluetooth receiving message. How do I check message received at board level?
Using the NUCLEO-WBA52CG I have been trying to get debug logs to be set over SWO(PB3). Using a logic analyzer I can see the logging getting to CN4:10(PB3/SWO). The signal does not make it to the embedded STLINK-V3MODS pin 6. There are notes in the de...
Hi, I need NUCLEO-WBA52CG boards schematics and Bill of materials. So it will be useful for me to replicate/use/create circuits as far my concern.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.