NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
We are working with the STM32WB series for Bluetooth communication and need to assign specific Bluetooth MAC addresses to our devices during End-of-Line (EOL) testing. Instead of using the default factory-assigned MAC address.What is the recommended ...
Hi, I was wondering if there's any update on when "Matter Ethernet Examples" might be available. Looking forward to it. https://wiki.st.com/stm32mcu/wiki/Connectivity:Matter_develop_and_prototype#Platforms_supporting_Ethernet_technology Regards
Hello team, I am Manikandaprabu from illuminen technologies. I am working with STM32WB55CGU7 for client, server application.We need to pair the client and server modules and find the distance. Now we developed, client and server pairing is ok but th...
- MRSUBG is disabled in CubeMX if i disable LSE , - CubeMX allows me to use MRSUBG only if i enable LSE. Is that possible to use MRSUBG with LSI ?
I'm trying to create a ZigBee-only project (no BLE), that will only implement an APS Coordinator with FreeRTOS support for the STM32WB5MMG module. I'm looking at the Zigbee_APS_Coord sample, which is exactly what I need, and I noticed that it has a f...
Hello,Please i have question.for the board : NUCLEO-WB05KZ : Can I program this board with arduino IDE? If you have simple tutorial codes for BLE to get you started, please let me know.Thanks
My supervisor and I have been trying to do some work using the Seeed studio board LoRa-E5 mini using STM32WLE5JC. After struggling a bit with removing the included write protection using the STM Programmer and a ST-Link, we managed to upload a script...
Hello all.I'm writing an application using an STM32WL33 device, actually facing continuous problems related to the documentation and SDK, that seems to suffer (understandable) youth issues.After having solved many, I came now to several problem I can...
I have a application where stm32wb5mm is acting like a beacon. I got it to advertise configured data, now I am trying to advertise temperature measurement, for this, I need to dynamically update advertising data packages. So my advertising works ok, ...
Hello,I am working on a project using Nucleo-WL55JC1 and the X-NUCLEO-IKS01A2 sensor board. My goal is to read sensor data (temperature, humidity, pressure, etc.) and send it over LoRaWAN to a network server such as ChirpStack.I have already connecte...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.