2019-04-30 9:44 AM
Hi,
the program does not start if I connect a second usb power supply (or external power supply). The MCU runs normally when a st-link is connected. I tried a simple program - LED blink. The voltage on the MCU is good and the power LD6 is on. Any fuse or lock?
Thank you
2019-04-30 10:02 AM
Make sure you have current ST-LINK firmware, and that NRST is not being held low.
2019-04-30 10:28 AM
ST link FW is new V2.33.25 now and NRST is high. It runs normally if both power are connected. The program will stop if I disconnect the st-link. The LED stays on (only stop - no reset).
2019-04-30 11:06 AM
What are you configuring as a clock source? 8MHz HSE?
2019-04-30 11:24 AM
I use internal HSI 16 MHz. The board has no soldered external crystal
2019-04-30 11:34 AM
The ST-LINK supplies an 8 MHz signal, the Murata has an 32 MHz TCXO
Run these things from batteries here. Check jumper settings.
Perhaps output diagnostics via a UART so you better understand what's happening internally.
2019-04-30 12:47 PM
ok, I'll try to find something
Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.