2021-06-08 12:15 AM
2021-06-08 3:28 AM
Hi,
What is your question exactly ? Does the Nucleo-G070RB supports the X-Nucleo-GFX01K1 display ? If yes, then it does. Since you added the TouchGFX tag I suppose you are wondering if it will work with TouCHGFX ? The answer is also yes, but there are no application templates available in TouchGFX Designer. You can have a look at the application template for the STM32G071-nucleo board, which uses the X-Nucleo-GFX01K1 display, and use it to configure your project.
/Romain
2021-06-08 3:28 AM
Hi,
What is your question exactly ? Does the Nucleo-G070RB supports the X-Nucleo-GFX01K1 display ? If yes, then it does. Since you added the TouchGFX tag I suppose you are wondering if it will work with TouCHGFX ? The answer is also yes, but there are no application templates available in TouchGFX Designer. You can have a look at the application template for the STM32G071-nucleo board, which uses the X-Nucleo-GFX01K1 display, and use it to configure your project.
/Romain
2021-06-08 6:50 AM
KK.Thank you.
2021-06-08 10:58 PM
Hello Kkanu.1,
When your question is answered, please close this topic by choosing Select as Best.
/Alexandre
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.