2017-10-17 6:58 AM
According to
, STM32F4 includes DSI interface with up to 2 lanes. See page 15.I am wondering if there is any MCU with 3 data lanes (L0, L1, L2) and CLK lane?
#stm32f4 #dsiSolved! Go to Solution.
2017-10-17 10:08 AM
Hi
rostokus
,Unfortunately,there is no STM32 device with 3 DSI data lanes, the STM32 embeded maximum 2 data lanes.
-Nesrine-
2017-10-17 7:16 AM
Posted on October 17, 2017 at 16:16
Hi rostokus,
The STM32F469/479 devices embeded MIPI® DSI host controller supporting up to 720p 30Hz resolution.
The DSI Host provides a scalable architecture using one or two data lanes.The number of lanes depends on the bandwidth requirements of the application. Each DSI lane has a maximum of 500 Mbit/s data rate, for a total 1Gbit/s rate in dual data lane mode.
Further information are detailed in AN4861application note it may help you.
-Nesrine-
2017-10-17 9:29 AM
Hi Nesrine,
You said 'using one or two data lanes'.
But my questions is whether you have any MCU with three data lanes?
Recommended app note does not mention about 3 lanes (only two)
Thanks
2017-10-17 10:08 AM
Hi
rostokus
,Unfortunately,there is no STM32 device with 3 DSI data lanes, the STM32 embeded maximum 2 data lanes.
-Nesrine-
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.