2020-04-18 2:02 PM
Hello,
I want to update my display data via SPI DMA. The display has 480x320px and I have chosen a 3 bit color coding, so that I can send two pixel within one byte. So my framebuffer has a size ox (480x320)/2 = 76800 byte. But when I want to transmit them with
HAL_StatusTypeDef HAL_SPI_Transmit_DMA(SPI_HandleTypeDef *hspi, uint8_t *pData, uint16_t Size)I have the size restriction. Do you have any idea how to solve this? I tried to use a state machine within the Interrupt:
switch ( eSpiDMA_TransmissionState )
{
case eStartTransmission:
LCD_CS_SET;
LCD_DC_RESET;
LCD_CS_RESET;
eSpiDMA_TransmissionState = eSendFirstHalf;
if ( HAL_SPI_Transmit_DMA( &hspi2, (uint8_t *)0x2c, 1 ) != HAL_OK)
{
// todo: error handling
}
break;
case eSendFirstHalf:
LCD_CS_SET;
LCD_DC_SET;
LCD_CS_RESET;
eSpiDMA_TransmissionState = eSendSecondHalf;
if ( HAL_SPI_Transmit_DMA( &hspi2, &displayFramebuffer[0], 38400U ) != HAL_OK)
{
// todo: error handling
}
break;
case eSendSecondHalf:
eSpiDMA_TransmissionState = eStartTransmission;
if ( HAL_SPI_Transmit_DMA( &hspi2, &displayFramebuffer[38400U], 38400U ) != HAL_OK)
{
// todo: error handling
}
break;
}But this doesn't work (it seems that the display is updated in 4 instead of 2 parts), and doesn't update afterwards ( I change the color in another task every 500ms, but the display color doesn't change).
Any ideas for this?
2020-04-18 8:09 PM
Set it up to transmit half or full words instead of bytes. That way the number of transfers is below 65536. I know the peripheral will allow this. Pretty sure HAL will do it too.
2020-04-19 11:49 AM
Hello,
unfortunately I have some problems getting the display running when running in 16bit mode (can't find out why since I don't have an oscilloscope).
2020-04-19 1:24 PM
I tried to build a union with the 8 bit framebuffer array (that's easier for me with my graphical lib) and a 16bit array for dma. After the configuration of the display I sitched to 16bit SPI and tried to send the data:
hspi2.Init.DataSize = SPI_DATASIZE_16BIT;
if (HAL_SPI_Init(&hspi2) != HAL_OK)
{
Error_Handler();
}
LCD_CS_RESET;
LCD_DC_SET;
HAL_SPI_Transmit_DMA( &hspi2, (uint8_t*)imageFramebuffer.displayFramebuffer16Bit, 38400U );but it only sends the data as 8 bit (every second pixel is blank, image is streched).
Do you have any idea?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.