2023-08-17 5:07 AM - edited 2023-08-17 5:45 AM
I am using STM32H750VB Custom Board. It has 16bpp parallel RGB interface with an TFT LCD of resolution 800x480. As I have no external memory, I am using RAM_D1 of 512KB as framebuffer resulting in, as per the calculation, resolution area of 800x300 in TOUCHGFX screen. Single buffer with allocation by address(0x24000000) is used in CUBEMX.
QUADSPI flash used is of 16MB and have created partition of 2MB of application code and rest for the asset of TOUCHGFX . Every precaution which needs to be taken care of in LD file is done.
When the code is generated, touchgfx_taskEntry(); is called from TouchGFX_Task(); which contains hal.taskEntry(). Have modified taskEntry() as given below in TouchGFXHAL.cpp :
void TouchGFXHAL::taskEntry()
{
enableLCDControllerInterrupt();
enableInterrupts();
OSWrappers::waitForVSync();
backPorchExited();
for (;;)
{
OSWrappers::waitForVSync();
backPorchExited();
}
}
TouchGFX_Task() specifications are:
priority :ospriority normal
stack size : 4096 words
code generator : external
parameter, buffer name, control block : NULL
Allocation : Dynamic
There are two other tasks along with TouchGFX_Task(). They are default task and idle generated by the software itself.
Other two tasks are running but TouchGFX_Task()(called only once).
So problem is, this gets called only once.
Also, one major problem I noticed is that TouchGFXGeneratedHAL::endFrame(); is not called.
Can anyone please help me with this?
CUBEMX VERSION : 6.9.1
CUBEIDE VERSION : 1.13.1
TOUCHGFX VERSION : 4.22.0
2023-08-17 9:21 PM - edited 2023-08-20 9:14 PM
I need the solution please someone help.
2023-08-20 9:12 PM - edited 2023-08-20 9:15 PM
Can anyone please help with my Custom Board?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.