2025-09-08 5:07 AM - last edited on 2025-09-08 7:14 AM by mƎALLEm
Hi Community,
We are exploring the migration of our FreeRTOS-based firmware to Zephyr. Our current design heavily relies on TouchGFX (provided by ST) for controlling an 800×480 touch display.
Here are some key details of our setup:
Is there any sample application or detailed documentation available for achieving this on Zephyr?
I have already briefly reviewed the following resources:
However, I need more guidance, specifically:
We have a tight project deadline, so I need to quickly determine:
Any insights, references, or experiences would be greatly appreciated.
Regards,
Devanshu Agarwal
2025-09-08 6:15 AM
We have internal proof of concept of this, and are working towards a way to handle documentation and release of an example project or two.
At the same time, Zephyr is not a supported target for TouchGFX, so there will be some things we cannot help you with here.
I will check if we can share one of the proof of concept projects at this stage.
The simplest way to get your setup to work should be to get the QSPI flash memory and maybe your FMC RAM mapped in Zephyr, and handle the rest of the peripherals you listed in the STM32Cube driver port for Zephyr. You will need to do the LTDC this way to be able to register an interrupt handler, and for DMA2D there is no Zephyr interface.
You will need to enable the specific driver files you need to include as Zephyr modules and disable the peripherals from device tree, and then you should be able to copy the code from your old main.c into the zephyr main.c, along with relevant code for each peripheral from you hal_msp.c file.
You will also need to register some interrupt handlers(LTDC and DMA2D, at least), they should just call the HAL interrput handler, just like the _it.c file from your CubeMX project does, then TouchGFX will either override the callback or register a callback function to them.
When all the peripherals are enabled, you can copy your entire TouchGFX folder from your old project into the Zephyr project. You will need to create a Cmakelist.txt for TouchGFX and include that in your Zephyr application.
You can enable a CMSIS wrapper in Zephyr, this will enable you to reuse your oswrapper file from your FreeRTOS project. Main should start a thread that calls TouchGFX_Task().
There is a bit too much to detail here, and I'm not sure it would be all that easy to glean all of it from an example project anyway, since it will always be a somewhat weird mix of a Zephyr project that has been massaged to be able to fit a TouchGFX project inside.
I will try to get a project cleared for sharing with you, but the first step should be to get your peripherals initialized and confirmed working in Zephyr. Even with the example project there will be details that I have forgotten, but I will try to help to the best of my ability.
2025-09-08 9:31 PM
Thank you for the prompt response and clear explanations. It would be greatly appreciated if you could share the project with us. We'd like to quickly test, modify, and validate it on an evaluation/development kit to better understand the porting efforts.
2025-09-10 1:13 AM
I will be able to share a proof of concept project for the STM32U5G9J-DK2 discovery kit, but I will need to make some small changes and cleanup before it is ready for sharing. I will try to prioritize this task as soon as possible.
In the mean time you could consider acquiring the board if you want to be able to run the sample project.
2025-09-18 8:29 AM
Here's the project for the U5G9-DK2.
It should be placed in a Zephyr workspace and can be built with west build -b stm32u5g9j_dk2 app --pristine auto from the root of the project. Flash using west flash. Alternatively, the run target button in the TouchGFX designer builds and flashes automatically. External memory is supported, and an external loader is supplied and used by west flash.
The LTDC, CRC, DMA2D and GPU2D are initialised using STM32 HAL code, all other peripherals including the touch screen is handled in device tree.
The LTDC can also be initialised using device tree, it is disabled in board overlay, but the display driver captures the line interrupt which is needed by TouchGFX. I'll work on a solution to this before publishing the final project and documentation, but this works well for now.
Have a look at prj.conf, there are some things that are crucial for the project to work there.
2025-09-19 8:18 AM
Hi,
Thanks for sharing the sample project and steps. We will refer to it and make changes for our STM32H7 dev board. I will reach out to you if we need further help. Thanks again.
Regards,
Devanshu Agarwal
2025-11-16 8:58 PM
Did you get the chance to get this working with LTDC configured via device tree. I am seeing the issues of interrupt handling needed by TouchGFX.
Also, is it possible for you to share this sample application with STM32H745. We are on a tight schedule and need to get this running soon.
Regards,
Devanshu Agarwal
2025-11-17 1:33 AM
We do not have any sample application for H7, I'm afraid.
If you want to initialize the LTDC from device tree, you either need to modify the LTDC driver to call some function in your code that calls the LTDC HAL callback handler or disable the interrupt handling in the driver. I have been working on adding this in upstream Zephyr, but I do not currently have the time, it is not a primary focus for me at the moment.
You can also hack it by adding the following in a device tree overlay:
<dc {
interrupts = <0 0>, <89 0>;
};This way, the Zephyr LTDC driver will trigger on interrupt 0, which is Window Watchdog interrupt, instead of the actual LTDC interrupt. If you use that interrupt, you should use another number that is unused, you can find the table for the interrupts and their position numbers in the reference manual for your MCU.
That will free up the LTDC interrupt to be handled by you manually - it should just call the LTDC HAL callback handler like in my example. The interrupt handling in the Zephyr driver is not useful, TouchGFX handles that part internally.
2025-11-17 3:34 AM - edited 2025-11-17 3:34 AM
Ok. Thanks for the update.
I tried building the sample application that you shared for STM32U5g9 but it is not working for me. It gives me the following errors:
/workdir/apps/TigerZephyrTBS/app/TouchGFX/lib/touchgfx/lib/core/cortex_m33/gcc/libtouchgfx-float-abi-hard.a /workdir/apps/TigerZephyrTBS/app/TouchGFX/lib/touchgfx_components/gpu2d/NemaGFX/lib/core/cortex_m33/gcc/libnemagfx-float-abi-hard.a /workdir/apps/TigerZephyrTBS/app/TouchGFX/lib/touchgfx_components/gpu2d/TouchGFXNema/lib/cortex_m33/gcc/libtouchgfxnema-float-abi-hard.a zephyr/arch/common/libisr_tables.a -mcpu=cortex-m33 -mthumb -mabi=aapcs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mfp16-format=ieee -mtp=soft -fuse-ld=bfd -Wl,--gc-sections -Wl,--build-id=none -Wl,--sort-common=descending -Wl,--sort-section=alignment -Wl,-u,_OffsetAbsSyms -Wl,-u,_ConfigAbsSyms -nostdlib -static -Wl,-X -Wl,-N -Wl,-no-pie -specs=picolibc.specs -DPICOLIBC_DOUBLE_PRINTF_SCANF -L"/opt/zephyr-sdk-0.17.4/arm-zephyr-eabi/bin/../lib/gcc/arm-zephyr-eabi/12.2.0/thumb/v8-m.main+fp/hard" -lstdc++ -lc -lgcc && cd /workdir/build/TigerZephyrTBS/app/zephyr && /usr/bin/cmake -E true
/opt/zephyr-sdk-0.17.4/arm-zephyr-eabi/bin/../lib/gcc/arm-zephyr-eabi/12.2.0/../../../../arm-zephyr-eabi/bin/ld.bfd: app/libapp.a(app_touchgfx.c.obj): in function `MX_TouchGFX_Init':
/workdir/apps/TigerZephyrTBS/app/TouchGFX/App/app_touchgfx.c:68: undefined reference to `touchgfx_components_init'
/opt/zephyr-sdk-0.17.4/arm-zephyr-eabi/bin/../lib/gcc/arm-zephyr-eabi/12.2.0/../../../../arm-zephyr-eabi/bin/ld.bfd: /workdir/apps/TigerZephyrTBS/app/TouchGFX/App/app_touchgfx.c:69: undefined reference to `touchgfx_init'
/opt/zephyr-sdk-0.17.4/arm-zephyr-eabi/bin/../lib/gcc/arm-zephyr-eabi/12.2.0/../../../../arm-zephyr-eabi/bin/ld.bfd: app/libapp.a(app_touchgfx.c.obj): in function `TouchGFX_Task':
/workdir/apps/TigerZephyrTBS/app/TouchGFX/App/app_touchgfx.c:87: undefined reference to `touchgfx_taskEntry'
collect2: error: ld returned 1 exit status
ninja: build stopped: subcommand failed.
FATAL ERROR: command exited with status 1: /usr/bin/cmake --build /workdir/build/TigerZephyrTBS/app
user@c97e638a0182:/workdir$ In this same setup, I am able to build the other sample applications provided by Zephyr thus ruling out my setup as the issue.
Attaching logs for your reference.
Can you please help check what I am missing?
2025-11-17 3:52 AM
I think you will need to open the project in TouchGFX designer and generate code.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.